I need to make an interaction calculation between a cast-in rail and some extra drilled anchors to take-up complementary // forces

Geplaatst door Pierre Lombaover 3 years ago
I need to make an interaction calculation between a cast-in rail and some extra drilled anchors to take-up complementary // forces

Configuration : plate with an underdimensionned cast-in rail as the previous engineer forgot in-plane loads.

The solution is to increase the plate dimension and add two extra drilled anchors in slotted holes.

How to model a slotted hole in a sofa configuration (it seems it's activated by applying filled holes while I'll need slotted holes to limit interferences between the rail and the drilled anchors)

SOFA,Complementary anchors,Cast-in interaction with drilled anchors

1 Antwoord
Geplaatst door Hilti Belux Engineering Team!over 3 years ago
Antwoord geaccepteerd

Hey Pierre,

Thank you very much for asking the question through Ask Hilti!
SOFA is a design method that goes further than the eurocodes. It is applied when the anchor configuration is not described in the norm. A possibility is to change the anchor configuration into one that is described in the norm and with slotted holes.

If this is not an option for your project, please contact us via Belux.engineering@hilti.com and send us the PE-file so we can find other options!

Kind regards,
Belux Engineering Team

Profis Engineering,Eurocode 2,Anchors,SOFA,Complementary anchors